Hi,
We are using BQ25100 for charging in our battery based solution. We see Iset pin is used to control charge current. Can the ISET pin be used to detect when the charging is complete? The reason is that while monitoring ISET using ADC pin we can clearly see the correlation between current pumped in by charger to the voltage measured on ISET. When battery reaches its maximum voltage the current(and hence voltage on ISET) starts dropping and after a while settles at state of not charging. Could you confirm this behavior and if we could use this as detection of when charging is finished