I'm working on a design with a 5V LM25116 based regulator with an intended current limit of 4A which has 5V output. To achieve this, I'm getting nearly 40mOhm of shunt requirement which becomes the dominant power loss of around half a watt. The shunt gets far hotter than any other component during operation.
This is not really acceptable to have the dominant loss be a sense element. Is there anything I can do to keep the current limit with a lower shunt? Presumably I could add an external amplifier but that would be a major revision to the design. Are there any tricks with external resistors to increase the gain or increase the offset above the internal 0.5V? Or lower the 1.6V overcurrent threshold?