Hi,
can the LM5010 or LM5010A be used as a fly-buck converter?
In my case Vin=36V(18-72V), Vpri = 15V (200mA) Vsec = 5V(400mA)
If LM5010 does not meet the demand if I can use LM5017
Kind regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.