I'm attempting to configure the TWL4030 in "Mode 2" - one Audio + one Voice
When I attempt to configure the OPTION Register, I can't set any of the Audio Enable bits (0, 1, 5, 6 or 7).
Am I missing something?
Is this a bug?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm attempting to configure the TWL4030 in "Mode 2" - one Audio + one Voice
When I attempt to configure the OPTION Register, I can't set any of the Audio Enable bits (0, 1, 5, 6 or 7).
Am I missing something?
Is this a bug?
Did a bit of testing - it looks like the Audio bits in the OPTION register can only be set after the CODEC_MODE CODEECPDZ bit is set.
Does this make sense?
Hi,
This should not be the case. Please refer the programming sequence in the audio chapter for TPS65950.
Regards,
Gandhar.