This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40z50-r1 CRC PEC

Expert 1635 points
Other Parts Discussed in Thread: BQ40Z50

Hi,

I am required to verify the data integrity in the SMBus connection between an MCU and a BQ40Z40-R1.  There are no specifics in the documentation I read and I would like to know how should it be implemented for the following two cases, with the MCU being the master in both:

a) When reading a byte from the gauge, and

b) When reading a word.

I would appreciate information on the appropriate CRC table, necessary BQ40Z50 configuration and the procedure itself.  Thanks.

Pibe

  • This question was never responded by TI. In the meantime I got some information from a colleague that all the secret is to read back 3 bytes, either for one byte or a word.  In the case of the byte reading the second byte will be a zero. In both cases the third byte is the CRC8.  The table used for the calculation is:

    uint8_t crcTable[256] =
    {
        0x00, 0x07, 0x0E, 0x09, 0x1C, 0x1B, 0x12, 0x15, 0x38, 0x3F, 0x36, 0x31, 0x24, 0x23, 0x2A, 0x2D,
        0x70, 0x77, 0x7E, 0x79, 0x6C, 0x6B, 0x62, 0x65, 0x48, 0x4F, 0x46, 0x41, 0x54, 0x53, 0x5A, 0x5D,
        0xE0, 0xE7, 0xEE, 0xE9, 0xFC, 0xFB, 0xF2, 0xF5, 0xD8, 0xDF, 0xD6, 0xD1, 0xC4, 0xC3, 0xCA, 0xCD,
        0x90, 0x97, 0x9E, 0x99, 0x8C, 0x8B, 0x82, 0x85, 0xA8, 0xAF, 0xA6, 0xA1, 0xB4, 0xB3, 0xBA, 0xBD,
        0xC7, 0xC0, 0xC9, 0xCE, 0xDB, 0xDC, 0xD5, 0xD2, 0xFF, 0xF8, 0xF1, 0xF6, 0xE3, 0xE4, 0xED, 0xEA,
        0xB7, 0xB0, 0xB9, 0xBE, 0xAB, 0xAC, 0xA5, 0xA2, 0x8F, 0x88, 0x81, 0x86, 0x93, 0x94, 0x9D, 0x9A,
        0x27, 0x20, 0x29, 0x2E, 0x3B, 0x3C, 0x35, 0x32, 0x1F, 0x18, 0x11, 0x16, 0x03, 0x04, 0x0D, 0x0A,
        0x57, 0x50, 0x59, 0x5E, 0x4B, 0x4C, 0x45, 0x42, 0x6F, 0x68, 0x61, 0x66, 0x73, 0x74, 0x7D, 0x7A,
        0x89, 0x8E, 0x87, 0x80, 0x95, 0x92, 0x9B, 0x9C, 0xB1, 0xB6, 0xBF, 0xB8, 0xAD, 0xAA, 0xA3, 0xA4,
        0xF9, 0xFE, 0xF7, 0xF0, 0xE5, 0xE2, 0xEB, 0xEC, 0xC1, 0xC6, 0xCF, 0xC8, 0xDD, 0xDA, 0xD3, 0xD4,
        0x69, 0x6E, 0x67, 0x60, 0x75, 0x72, 0x7B, 0x7C, 0x51, 0x56, 0x5F, 0x58, 0x4D, 0x4A, 0x43, 0x44,
        0x19, 0x1E, 0x17, 0x10, 0x05, 0x02, 0x0B, 0x0C, 0x21, 0x26, 0x2F, 0x28, 0x3D, 0x3A, 0x33, 0x34,
        0x4E, 0x49, 0x40, 0x47, 0x52, 0x55, 0x5C, 0x5B, 0x76, 0x71, 0x78, 0x7F, 0x6A, 0x6D, 0x64, 0x63,
        0x3E, 0x39, 0x30, 0x37, 0x22, 0x25, 0x2C, 0x2B, 0x06, 0x01, 0x08, 0x0F, 0x1A, 0x1D, 0x14, 0x13,
        0xAE, 0xA9, 0xA0, 0xA7, 0xB2, 0xB5, 0xBC, 0xBB, 0x96, 0x91, 0x98, 0x9F, 0x8A, 0x8D, 0x84, 0x83,
        0xDE, 0xD9, 0xD0, 0xD7, 0xC2, 0xC5, 0xCC, 0xCB, 0xE6, 0xE1, 0xE8, 0xEF, 0xFA, 0xFD, 0xF4, 0xF3
    };

    The calculation is something like:

    uint8_t crc = 0; crc_index = 0;

    uint8_t cn_bytes = 5;   // The whole exchange is 6 bytes long but the returned CRC is not computed

    uint8_t* cmd_resp points to an array containing the whole exchange (command and response): 0x16, register, 0x17, LoByte, HiByte/0, CRC8.

    while ( cn_bytes-- )
    {

           tbl_index = *cmd_resp++ ^ crc;
           crc = crcTable[tbl_index];
    }

    If crc == returned CRC8 in the response (3rd byte) then the exchange is good (or as good as an 8-bit CRC allows!)

    Hope this helps.

    Pibe

  • Hey .
    I also encountered a similar problem in BQ40z50
    In specifications they not explain how to calculate CRC when sended write command.
    I need a table that describe they correct CRC , and the code how to calculate it.
    thanks.