This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP7760 POWERSUPPLY TRANSFORMER DESIGN

Hi,

     I want to build a powersupply that takes 600V DC as input and 12V DC( 1A min ) as output.

pmp7760 design is okey for me. But i couldn't find the transformer( G094215LF from gci technologies) they are mentioning.

I have tried GCI website also but it is not there. So please say what are the specifications for the transformer.

Is there way to adjust the output voltage?. How they converted a 6V to 60V input IC into 800v input?