Hi,
My customer requests dimming resolution such as following file.
Can the LP8860-Q1 achive this dimming raio?
I think that it cannot achive 0.00172%/step, is it correct?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer requests dimming resolution such as following file.
Can the LP8860-Q1 achive this dimming raio?
I think that it cannot achive 0.00172%/step, is it correct?
Best Regards,
Kuramochi
Hi,
The min output PWM pulse width of LP8860 is 200ns, and min freq of PWM output is 4883Hz. The period of 4883Hz is ~200us.
200us/200ns = 1000. If you use hybrid dimming which current to PWM dimming switch point at 12.5%. Dimming ratio can be 8000.
Step size is another concept. If PLL freq = 40MHz as a sampling freq of output PWM, and PWM freq is 4883Hz, 40MHz/4883Hz = 8191(~13 bit)
If you use 3 bit steady dithering on top of this, 16 bit resolution(65535 steps) can be supported. 0.00172%/step = 58139 total steps.
In order to have clean 16 bit brightness input, using brightness register will be better to test this.
Hope this helps,
Hi Siwei,
SW frequency of LP8860 is independent from PWM resolution/freq.
Boost SW freq can be decided by SYNC(not VSYNC) input if external clock is used.
Hope this helps,