Hi,
LMZ21700 is rated for 0.9 < Vout < 6.0 under "Recommended Operating Conditions". Using the datasheet feedback equation RFBT = RFBB x (VOUT/ 0.8 – 1), it's possible to achieve Vout = 7.1V using:
Vin = 11.7V
RFBT = 44.2k
RFBB = 348k
In practice, Vout deviates by about 10% from calculations. Aside from this error, performance seems to be well suited for my application. A 5V LDO with 2V dropout is more economical than operating LMZ21700 at 6V with a 5V LDO specified for lower dropout voltage. Noise performance matches full linear regulation peformance in this system.
What are the potential production consequences of operating LMZ21700's output voltage above recommended conditions?