Hello,
I am evaluating BQ28Z610 with the EVM. I tried to put the device in SHUTDOWN mode via bqmanager.
The bq28z610 did went in shutdown (XCHG & XDSG = 1, then bqmanager loses connection), which is as expected as per the reference manual.
The issue is that the bq28z610 did never resumed normal operation. I pushed P4 (which sends P2 voltage to PACK+ and should wake the bq28z610) but it did not woke up.
I also disconnected completely the batteries and let the board sit all night but that did not change anything.
How can I fix this or prevent this issue?