I am working on a design that require outputs of 15VDC@3A and 5VDC@3A from an input of 24VAC which requires a half wave rectifier circuit only. I am concerned about how much of a smoothing capacitor I will need to get the TI power supplies circuits to work properly.
I roughly need 4700UF to smooth out the half wave rectified voltage when I may have as much as 3A of current required on the input. Even this may not be enough.
A 4700UF 63V capacitor is a lot bigger then I really want to use.
Does anyone have a example circuit or feedback on what the best approach would be for this?
How much ripple can I allow on the input of the power supplies before the TI switching supply circuits can keep up?