This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir.
CSD17573Q5B can replace competitor MOSFET CED93A3 ( TO-252 ) ?
Can suggest how to PCB layout for CSD17573Q5B, if we need Id current 100A ?
| Supplier | Version | Part No | Package | Outline | Id | Ch | Vds | Vgs | R@10V (Typ) | R@10V (max) | R@4.5V (Typ) | R@4.5V (max) | Qg@4.5V (typ) | Qgd@4.5V (typ) | TI PN |
| TI | CSD17573Q5B | QFN 5x6 | 5x6 | 100 | N | 30 | ±20 | 0.84 | 1 | 1.19 | 1.45 | 49 | 11.9 | ||
| CET | CED93A3 | TO-252 | 125 | N | 30 | ±20 | 2.5 | 3.2 | 4.2 | 6.2 | 60 | 25 |