Hello Sir
I use UCC27531 in a 1.5kW PFC circuit as MOSFET drive working together with UCC28180, The IN pin connects to the Gate pin of 28180 via a 100ohm resistor, while the gate of MOSFET is connected to the OUTH pin via a 10ohm resistor, and to the OUTL pin via a diode & 3ohm resistor. However, PFC can only output a power of about 400W. UCC27531 damaged (no output) when the power was going over 400W. The UCC27531 is biased with the same 15V power supply as UCC28180, and shares the same control ground with UCC28180. What might be the renson of the failure ?
best regards
xiaoming