This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z60: v13 to v15

Hi,

I want to upgrade a 4-cell v13 to a 4-cell v15.

The v13 looks heavyly modified compared to what is the default v13 on your web site.

Therefore I want to start from scratch.

First getting the default v15 to run and afterwards change to 4 cells.

Attached is a .srec file in .zip format.

The properties of the 4 cells are: 3.7v, 3900mAh, 14.43Wh.

Absolute minimum is 3000 mV. Absolute maximum is 4200 mV.

Thanks!

Have a nice day!

Regards,

Ivo

bq40z60EVM.zip