Can BQ40Z60 be used on the system-side? I am under the impression that this is a pack-side device. As such, I thought pack-side devices were designed to stay with the battery for the life of the battery. On the system-side, the fuel-gauge is designed to determine the state of charge on a newly inserted battery. Since BQ40Z60 uses the Impedance Track algorithm, it seems this part should be capable of being used on the system-side. I would like to confirm this case as well as understand any issues that may arise as a result. The reason I ask is that I have a customer wanting to use this device because it is a low cost integrated device, but his application is a system-side application.