I would appreciate any information I can get about using the BQ24104 chip to manage 3- Li-Ion cells.
I am powering two small device in a case.One Raspberry Pi and One 3 port USB 2.0 powered hub.
I am planning on using UltraFire 4000 mAh batteries with 3 in series with 2 sets of three in parallel, That should allow 8000 mAh of available current.
When accessing the information about the BQ24104, I do not see the circuit schematic for 3 cells.
I need to know if this chip will accept the current to charge two series of 3 cells?
Where can I go t get this information? Thank you for help.