Hello,
I am in need of a buck-boost switching regulator with the following requirements:
- 8-36V input voltage
- 12V output voltage
- 15A output current
Is it possible to use the LM5118 for this task?
I thought about using some FETs with Ron < 4mOhm. What is the max. allowed Qg for using a FET with the LM5118 in this application?
Which maximum switching frequency can I use?
Regards,
Niels