We are working on a board that uses the TPS25910. As part of the setup we are connecting the board to a Keithley 2306 Battery/Charger Simulator. The “supply” and sense lines of the Keithley are only connected to the TPS25910: IN, GND, EN (Pull-up to IN via 10K resistor) pins on the board.
We have encountered a behavior that we have not been able to root cause. When the board (not powered, or connected to anything) is connected to the Keithley 2306 in charger mode, we have a current drain ranging from 65mA to 200mA and what seems to be an oscillation. This does not occur when using the 2306 in battery mode or standard power supplies (not battery/charger simulator).
We wanted to find out if the TPS25910 may react differently when a “charger” is connected to the input pins than when a battery is. Is there anything on this setup that may be causing the behavior described?