I am using PMP7605 module as a reference design for street lightening application. This module can be used for 12 volt, 24 volt as well as 48 volt system and can be used for 10 amp, 20 amp as well as 40 amp. I have already gone through the design equation used for designing buck regulator in one of the application note snosb84c. But i am NOT very sure which value (Vin range, Vout, Iout, switching frequency) is considered for finding out Inductor and output capacitor value in PMP7605. As per design L = 10 uH and Cout = 1000 uf. But this value doen't matches with my calculation
i will be using same schematic and component but my requirement of MPPT charge controller is as mentioned below:
Solar Panel = 12 volt
battery = 12 volt
Iout = 10 amp
Can anyone please help me in the design calculation as which range of value is considered for designing PMP7605 and as per my requirement what could be the inductor and capacitor size.
It's urgent. Please help