Hi.
We have been using the BQ25504 for a while and it performs well.
But now we have reached the maximum input current from the solar cell which forces us to find another solution / IC.
The problem is that we are only using one cell (300-500mV), and the current handling of the IC is the limiting factor.
So my question is.
Is there any new IC/devices in the pipline that can handle higher current then the BQ25504 ?
Or do anyone have a idea about another solution for our problem ?
Best // Mike