I am considering using a supercap on the battery charging circuit, but understand that it will appear as a shorted output. Will this work? What I want is a way to provide uninterruptible power to a 5VDC powered digital system, based on the AM3358.
The main idea being to initiate a power fail mode, where filesystems are put into a stable state before power disappears completely. I want to prevent database corruption at the sudden loss of DC power and need a backup to do so. It only needs to work for a short time, but needs to charge quickly.
I am using the TPS65217C. Would a small battery be a better choice?