Hi,
Please let me know about TPS24750.
During normal operation, if VIN is short-circuit, output voltage is higher than VIN.How much the reverse current to allowable of body diode?
Regards,
Nagai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please let me know about TPS24750.
During normal operation, if VIN is short-circuit, output voltage is higher than VIN.How much the reverse current to allowable of body diode?
Regards,
Nagai
Hi Nagai-san,
For the reverse current blocking feature you can implement the design with an external N-FET as shown in Figure 46 in the datasheet. When Input supply get short circuited, the reverse current from output side will get blocked with this implementation. However there will be a transient reverse current through the FETs. Please select a logic gate level external FET with VGSth < 1.5V for the design (example: CSD17553Q5A). This will help to reduce the transient time for the reverse current through the body diode of the internal FET.
The internal FET can handle 20 A of transient current.
Regards,
Dilip