Please let me know about Power dissipation (= Thermal resistance) of TPS563201 below.
①Datasheet written in Rθja: 92.6℃/W and operating temprange are 125℃_max.
But, in the condition of 3.3Vout / 3A @eff:86%, Tj will over than Maximum rating.
Is it correct?
②TPS563201 simulated on webench, Rθja result was 62.9℃/W.
What's the difference?
Best regards,
Satoshi