We are using BQ24780SRUYT in the new revision of a consumer steam therapy product.Can we get some support as we test corner case power delivery? Planning to bring to market in 2016 Q4 EAU 20k units.
- What is maximum duty cycle?
- We are a battery operated system and need to validate ability to deliver proper power to our resistive load at Vin minimum. Is there a limit to the duty cycle for this part that is preventing our low dropout high power operation?
- Can we disable ULVO?
- We are using this part to drive a)resistive heater and b) recharge our batteries. When we operate the heater the UVLO trickle charge is enabled, limiting Iout to 500ma until Vout >2.4V! Can we get a part that does not have this UVLO level trip battery (we are having success adding a soft start to a high side switch but this is not ideal).