This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3429 for sepic circuit frequency instability .

Hello , I met a problem that i used lm3429 for sepic circuit ,the frequency is not stable  , when  change output current , frequency would became bigger .

and i used formula  frequency = 25/Rct *Crct ) =25/(47000*0.000000001)=531K,but measured frequency is 230K . I  cant figure it out  why frequency is strange..

Input voltage is 9 to 16v ,output is 12V,1A.  thanks for you help in advance .