I am using a BQ 24165 to switch between a Lead acide battery and a lipo battery. The led acid battery is arranged in a way that a DC DC is bring 5V from it into the BQ24165.
The Q24165 can not output more than 4.2V as this is a buck converter. I need to bring back 5V power rail with a current availability around 2.5A, what boost converter should I choose for this ?