HI,
Attached is v13.srec.
I use 4 cells, 3900mAh, 3,7V, 14,43Wh.
Absolute minimum 3000mV and absolute maximum 4200mV.
The 4-cell pack does charge and discharge, although both give up too soon.
End of charge the cells have around 3800mV and discharge gives up with 8% on the dial.
Learning Cycle never ends normally.
What am I doing wrong?
Thanks!
Regards,
Ivo