This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160

Other Parts Discussed in Thread: TPS54160

I am attempting to generate the design requirements for the TPS54160 and am defining the equations for frequency found on page 24 of the data sheet (equations 12 and 13).  I need to know the value for Vout(sc) (output voltage during a short).  I have completed the calculations using 0V as a worst case scenario but know that can't be right because I come up with a maximum frequency of 127.5kHz and TI webench has a maximum of 584.615 for a 50V input 3.3V output 0.5A  output.