Hello everyone,
I have a device i need to power with 1.0 V. It's sensitive to voltage supply variation. I'm concerned to use TPS62770 for this matter. According to the datasheet, the accuracy of Vout is -/+ 2.5% which very fine to me. However. My device is going to be power gated where Toff=4ms and Ton=4µs (D=0.1%) by controlling an SPDT put between the TPS62770 and my device . Now the transient behavior of the supply voltage TPS62770 is unclear to me in this situation. Given that my device will have some 100 ns inrush current. My question is how is TPS62770 going to maintain this voltage output (Step-down) accuracy in this situation? If I use the integrated step-up, lose the SPDT and use the EN2/PWM pin to perform the power gating. Then, Vout2 will be used and i will have to adjust the voltage by means of the voltage divider which can also be inaccurate. Please enlighten me.
Thank you,