I'm using the BQ24055 Evaluation Board with a 3.7V/2000mAh-battery. The configurations regarding to the IN, ISET, VSS, PRETERM, TS and ISET2 pins are set as follow:
Everything seems to be working just fine, except the charging function. The Power Good LED indicates correctly when the voltage input drops below the battery voltage, the IC's pins go to a high-impedance state when voltage input is higher than 6.6V, charge function is disabled when TS pin is pulled down and the CHG LED also turns on with te PG LED. However, there's no current in the circuit and, therefore, no charging happening. Is there anything that I'm doing wrong and not seeing it? Is it possible that I had the bad luck to get an imperfect IC/Evalation Board? Thank you.