Hello Forum,
I have questions related to BQ25895 - keeping input voltage above 4.8V for different power sources by reducing battery charge current.
Datasheet naming that "Dynamic Power Management" (see page 19, 8.2.6.2 Dynamic Power Management)
The question is: how to set input voltage threshold (VINDPM) ?
There is some description (8.2.3.4 Input Voltage Limit Threshold Setting ) of datasheet, which is not very clear.
Specifically:
For default mode ( case 2. in datasheet, the same page 17) datasheet writes:
2. Relative VINDPM based on VINDPM_OS registers (FORCE_VINDPM=0) (Default)
When FORCE_VINDPM bit is 0 (default), the VINDPM threshold setting algorithm is enabled. The VINDPM
register is read only and the charger controls the register by using VINDPM Threshold setting algorithm. The
algorithm allows a wide range of adapter (VVBUS_OP) to be used with flexible VINDPM threshold.
Is any description of algorithm? I could not find in datasheet.
How it utilizes the VINDPM_OS value? Is it dependent on power source detection?
What I should load to get threshold 4.8V ? Is one setting correct for any detected types of power sources?
For Absolute mode :
Is it enough just to load VINDPM value into REG0D to have DPM working for all detected types of power sources ?
Is any bits need to set for DPM beyond FORCE_VINDPM ?
Your help in clarifying this operation is appreciated.