This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61025 load transient

Hi Team,

The system is like below.

Power Source = AA Battery 2 EA

Load Current = Continuous 300 mA & Peak Current 500 mA

 

There is very short period when the peak current happen in a cycle. When the peak current happen, the output voltage drop from 3.3V to 2.3V.

It lead to system reset.

it there have any method to maintain the output voltage?