I am trying to get a UC3525 PWM chip to sync. Need to know correct method. I have been applying ro rhw aync pin 3 a 3v positive going pulse that is 0.7 us wide running at 40 kHz so I can get 20 kHz at the outputs. This makes the outputs fall into sync but distorts and reduces the pulse width to less than their 50% max.Maybe I need to keep pin 3 high and pull it low for the 0.7 us pulse?