Hi,
A customer of ours recently evaluated the following EVMs with a TDK coil for a wireless charging application that requires Qi compliance:
BQ51050BEVM – Qi receiver
BQ500212AEVM – Qi charger
BQ500210EVM – Transmitter
WR221230-36M8-G – TDK coil
https://product.tdk.com/info/en/catalog/datasheets/wr_rx-coil-wr221230-36m8-g_en.pdf
Some preliminary testing with the BQ51050BEVM (Qi receiver) and the BQ500212AEVM (Qi charger) with TDK coil proves that it is able to transfer 400mW of power across a 1mm with a lateral offset of 5mm from the centre of the coils, which is a good result. However, the BQ500210EVM transmitter is unable to deliver 400mW of power to the BQ51050BEVM with the TDK Coil. Customer suspects this is due to the Tx coil inductance being much higher (A1 type, 24uH) in the older style transmitter (BQ500210EVM). Could you please confirm this is true or some other issues that need to be addressed?
Thank you.
Deejay