ON THIS PART DO YOU SEE ANY PROBLEMS USING THE PART IN
PARALLEL TO INCREASE OUTPUT POWER...................................
ON ILE INPUT EACH UNIT WILL HAVE A 1 OHM .5% TO EACH INPUT AHE ALL THE RESISTORS TIED TOGETHER AT THE OTHER END FOR THE
DRIVE SIGNAL , EACH OUTPUT WILL HAVE A 1 OHM .5% RESISTOR AND ON THE OTHER END ALL THREE RESISTORS WILL BE TIED TOGETHER
THAT WILL GO INTO THE GATE OF THE MOSFET. THE DRIVER USED WILL BE ISOLATED AND FOR THE TOP AND BOTTOM DRIVERS I WILL USE A PARALLEL ASSY. TO DRIVE THE MOSFETS IN HI & LO APPLICATION THE + 15.0VDC POWER WILL POWER THE POWER DRIVER GROUP AND AT THE TOP THE +15 VDC WILL GO THRU A DIODE AND T 10 OHM RESISTOR FOR THE VDD AND A .47uF CAP WILL BE USED FROM THE TOP SOURCE BUS TO THE VDD PIN OF THR OUTPUT DRIVERS
LET ME NO IF YOU SEE ANY PROBLEM DRIVING THE UNIT AS INDICATED ABOVE
THANKS,
WILLIE L. MCCAIN