Gentlemen:
I have a situation using the bq24123 charger to charge two Li-Ion cells in series. When I first started charging the pack, the charger behaved normally, the In-Progress status light came on, and the gas gauge (bq20z655) indicated that the pack was charging. When I came back to the pack after lunch, it should have been signaling between 50% and 75% charge, and either still have been in CC charge mode or have just switched over to CV mode.
What I found was that the pack was no longer drawing current, and instead of signaling fully charged (Complete indicator on), there appeared to be no activity. I checked the battery voltage, and it was nowhere near fully charged. Examination of the pack revealed that a jumper which I had soldered to the board to correct an artwork error had come loose from the pad. I replaced the jumper, but still got no charging of the cells. What I did see was the In-Progress (STAT1) output flashing at approximately 1 Hz.
What does this flashing indicate? I cannot see this type of indication called out in the data sheet.