Hi
I have a question about"TPS51123 DataSheet P24[Choose the Output Capacitor(s)]"
I want to know the ”ESR” values necessary for the output capacitor.
It does out value even using Equation 8 under the following conditions,
I not out value. There is a thing to be considered something?
■Condition
Vin=12V、Vout=5V or 3.3V、
L=3.3uH
SWf=245kHz
Best Regard
T Kishi