Hello,
In the PMP10748, there is the LM5060-Q1 and the LM74610-Q1.
The LM74610-Q1 is used for reverse polarity protection.
However , I think that the LM5060-Q1 can be used for reverse polarity protection.
Could you please let me know the reason why the LM5060-Q1 is not used for reveser polarity protection.
Is the reason that the PMP10748 need ORing control?
If we don't need ORing control, should we use LM5060-Q1 only for reveser polarity protection?
We need OVP and OCP protection, thus LM5060-Q1 is necessary.
Best Regards,
Ryuji Asaka