This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950

Other Parts Discussed in Thread: UCC28950

Hi

I’m using UCC28950 to implement a 2.1 kW phase shifted full bridge dc/dc converter. Since the output voltage is high 170V I’m not using synchronous switch instead I’m using ultra fast diodes. No the question is that should I just leave the OUTE and OUTF pin float and N/C? Or should I connect the DCM pin to VREF to  cheat the UCC28950 so that it assumes it’s always in DCM mode and so not generating any OUTE or OUTF signal. Or should I connect DCM pin  to GND?

Thanks