Dear TI employee:
I am doing a project now using the wireless charger. Is there any evaluation board or chip in TI which can let us use i2c to monitor the battery status or change the parameters?
Best regards,
Yang FAN
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI employee:
I am doing a project now using the wireless charger. Is there any evaluation board or chip in TI which can let us use i2c to monitor the battery status or change the parameters?
Best regards,
Yang FAN
Yang,
Some wireless receivers contain I2C, some do not. Those that do have I2C are wireless power supplies and not chargers. They have registers that have information related to the wireless power system.
If you need information regarding the battery, you need to go directly to a stand-alone charger (which will work with the wireless power receivers).
What information do you need?
Regards,
Dick
Fan,
1) Register Map:
A) The registers can be used to change the output voltage (Register 1, bits B0, B1 and B2). The default value is 500mV (0x01) for this feedback node. Changing the register will change the voltage appropriately, within its specified output range.
B) Frequency cannot be changed, only monitored. The TX determines the frequency.
C) Other registers can be used as shown in the register map section starting on page 22.
Note that the bq51221 is a wireless power receiver. It generates a voltage / current that can be used by the system. It cannot charge batteries on its own.
2) To determine what charger is appropriate, more information is required. What is the battery type? What is the charging voltage? This would possibly a better question for the Charger Forum.
Regards,
Dick
Dear Dick:
Thanks for your kindly reply. I am now doing a project which needs a very small wireless charger circuit for the wearable circuit. It also needs to monitor and control the process of the wireless power transfer process. My battery is shown below in the picture. Do you have any suggestion for the transmitter and receiver type? we should use as less chip as possible. Thank you very much.
Best regards,
Yang Fan
Yang,
Look at the bq51003 as the wireless receiver and the bq25100 as the charger. See TIDA-00318 for the solution.
Regards,
Dick
Yang,
Please look at the bq25120. It is an I2C enabled charger and Battery Management Unit. It should provide all the information you need.
Regards,
Dick
Yang,
I am not an expert on the TI selection for an MCU. The MSP430 is a very popular and easy to use solution that I have used in the past for projects.
You can get more information at the Micro-controller E2E forum: e2e.ti.com/.../
Regards,
Dick
Yang,
Look at the bq500212A. There is an application note on how to interface with I2C.
You cannot set the frequency or voltage on the transmitter. It will alter its frequency or voltage to deliver the power requested by the receiver. The items you can monitor are covered in the application note.
Regards,
Dick
Hello Dick,
Quick question - we have a product that uses multiple BQ500212A devices. We are doing a revision and I just saw the I2C interface document. (The datasheet should be updated to indicate that I2C is NOT factory reserved.)
Just wondering about address - do all devices have the same address or are they different? I'm wondering about giving us the capability to address individual chargers - it would really add to the functunality. They are "hardcoded" so I am assuming they are all the same but just wanting to confirm.
Thanks,
Kurt
Kurt,
You are correct, the I2C address is hardcoded into the bq500212A. The address is 0x14.
I'm sure you are aware of the TCA7408 I2C I/O expander that might help.
Regards,
Dick
Dick
Thanks! This would have been a "nice to have" type feature. We have almost 50 wireless chargers in the product so for now it's not worth it to create any sort of expansion bus.
Cheers,
Kurt