This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD rating: Machine model (MM)

Other Parts Discussed in Thread: TPS2051

Dear Sirs

What is the the ESD rating Machine model (MM) of the following TI part? thanks 

Description
IC POWER SWITCH (R) TPS2051BDGNR
IC POWER SWITCH (R) TPS22924CYZPR
IC POWER SWITCH (R) TPS22920YZPR
IC SWITCH (R) TS3A27518EPWR

BRS

NAT

  • Hi Nat,

    Sorry for the delay. For the TPS2051, the ESD rating for MM is 200V (page 4 of the datasheet).

    For the other 3, there wasn't an MM ESD test on the Datasheet, but I would ask this question in the "Load Switches and Power Path Protection Forum". 

    Best Regards,
    Aramis P. Alvarez