This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP38798 - more than(over) 50dB(@20kHz upto 800kHz)

Other Parts Discussed in Thread: LP38798

Hi all

Would you mind if we ask LP38798?

Our customer are looking the following specification's LDO; 

Vin=13V

Vout=12V

Iout=50mA

PSRR= more than(over) 50dB(@20kHz upto 800kHz)

Does LP38798 satisfy with above specification?(The data sheet shows the condition with Vin=6V, Vout=5V)

Or, if you have know the device which satisfy with above specification, could you let us know?

We do need your help.

Kind regards,

Hirotaka Matsumoto