I am building a wireless charger using the bq500412 and an A6 (3 coil) assembly.
Because the board has to be washed and soldering the coil wires would be a secondary operation, I would like to know if it would be a problem to use a connector on the board and a crimped terminal on the coil wires, such as a Fast On quick disconnect. This would avoid the need for secondary washing of the board.