Hi Support,
Need your help to advise on the additional quality and reliability data such as radiation (SEU, SEL) & vibration on the LM137k/883 and LM137H1PQMLV.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support,
Need your help to advise on the additional quality and reliability data such as radiation (SEU, SEL) & vibration on the LM137k/883 and LM137H1PQMLV.
Thanks.
That is an IEEE paper. You should be able to click the link and get to it.
If you have troubles loading it, do a web search on:
Single-Event Transients in Voltage Regulators
If that doesn't work, let me know and I will see if there is another way to get it.
LM137K/883 is a military grade product.
For the space grade version of this product, you want the JL137SYA. It has been in production for over 20 years.
The LM137JAN-SP comes in the TO-3 package and has an output current maximum of 1.5A.
For generic data for a product using the same fab process and using the same package, see the LM117K:
We do not offer a radiation tested version of this part and have not tested it.
The LM137QML-SP comes in the TO-39 package and has a 500 mA output. The parts are similar except for the current limit circuit.
SEE performance should be similar. I don't know about TID performance.