This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Discharge rate is too high

1674,2016-06-13 17:00:06,6696.776,25.3,16068,-162,50,SUCCESS
1675,2016-06-13 17:00:10,6700.777,25.3,16066,-162,49,SUCCESS

[snip]

22918,2016-06-14 16:36:31,91682.456,24.6,11752,-131,41,SUCCESS
22919,2016-06-14 16:36:35,91686.456,24.6,11770,-100,40,SUCCESS


Warning: Discharge rate is too high. High rate reduces ID detection accuracy, 10 hr rate is recommended. Total discharge time is less than 5 hrs, t_hrs=  -0.00111111111111111

That's almost 24 hours. 4643.v13.zip

Thanks!

Regards,

Ivo

  • Ivo,
    The pack was only at 4035mV / cell at the beginning of discharge and the program could not find a ChemID match. The cells need to be charged to their normal full charge voltage for the program to work properly. I am not sure why it said that the discharge rate is too high, but it should be okay.
    Tom