This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100 - Charted Average current not stable with pulsed load

Other Parts Discussed in Thread: BQ34Z100, BQ20Z65

BQ34Z100 - Charted Average current not stable with pulsed load.

Hi,

With a pulsed load of 500mA x 2s, 0mA x 2s, 1000mA x 2s, 0mA x 2s (Repeat) to TDA the charted log of Average current is as shown on the attached file.

The period of the waveform is approx. 300  sec. The yellow line is the calculated average ie 375mA.

The result is that over the course of the discharge we are approx. -20% out. If the discharge was constant it would be correct.

Any ideas what could be going on or if a setting could be changed to solve?

Thanks

Best Regards

Martin Gibbs