This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using Primary Batteries (chemistry = LiSOCl2) with BQ27510-G3

Other Parts Discussed in Thread: BQ27510-G3, BQ27510, BQ27320

I would like to use a battery fuel gauge (p/n:BQ27510-G3) to monitor the state of discharge of my battery pack, but I am using two primary batteries in parallel (TL-5930 from Tadiran, battery chemistry is Li-SOCl2).

First, I don't see LiSOCl2 chemistry listed, so I assume I have to run bqEASY and the ChemID tool.

However, this routine requires that I charge the pack, but I can't charge because I am using primary cells.

My questions:

1) Is there a recommended profile for Li-SOCl2 chemistry that may be "good enough" to monitor the battery life for my application?

2) Is there a recommended way to manipulate the bqEASY routine so that I can skip the charge portions and create a golden .DFI file for my pack?

I have tried researching the forum for similar posts (see links), but none of them directly address how I might be able to use the BQ27510 to monitor a primary LiSOCl2 battery. I have read that the p/n I have chosen was not designed for primary batteries, but I am willing to try anyways.

http://www.ti.com/lit/an/slua367/slua367.pdf

https://e2e.ti.com/support/power_management/battery_management/f/180/t/285620

https://e2e.ti.com/support/power_management/battery_management/f/180/t/271500

Thanks in advance for the help.

Matt