This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1 Overcharge Alert

Other Parts Discussed in Thread: BQ40Z50-R1

Hi Sir/Madam,

We are using BQ40Z50-R1 in battery pack design.

We are getting an OC (overcharge alert) even though the criteria for OC was not met.

Criteria: Remaining Capacity >= Full charge capacity and Internal Charge > 0

Our OC threshold is set at 456mA.

The OC alert happened during the test when:

Remaining Capacity = 4329mAh

Full charge capacity = 4373mAh

Voltage = 4.187V

Current = 735mA

Please advise. Thank you very much.