Switcher pro indicated that max duty cycle is too high, but this device should work with 100% duty cycle according to the data sheet.
Is switcher pro correct for 5.5 to 32 Vin application?
Vout is 5V @ 2A.
-------------------------------------------------------------------------------------------------------------------------------------------
Error building the design. The Designer could not successfully build an error free design with this device and these inputs.
Error: Maximum Duty cycle is too High for the device.This design will not work at Minimum Vin!
Design Halted.
************Detailed Design Event Trace************
Design TPS54260 32V to 5V @ 2A Started at 6/14/2010, 3:31:56 PM.
TPS54260 Selected for this Design.
Starting Design for Channel 0...
Basic Design Inputs:
Vout = 5.00
Iout = 2.000
VinMin = 5.50
VinMax = 32.00
Other Design Inputs:
--------------------------------------------------------------------------------------------------------