How was design PMIC TPS65217 power up using PB_IN turn on system ?
adapter plug in->push button->system on
Beaglebone Black's PMIC design is adapter plug and turn on system.
BR...
Hacker Hsu,
.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hsu,
The Beaglebone Black turns on immediately because the supply is 5V into the AC rail.
When the power source is just a battery on the BAT rail, a push-button press is required to start the system.
Are you designing a new system or debugging an existing one?
Hi Sir,
Yes, I am designing a new system about AM3352 process.
My customer is connecting power source on the BAT. But it is not work. It is pluging adapter and turn on system. PB_IN is not working.
BR..
Hacker Hsu,