Hi
We are using the UCC28070 PFC controller to implement an off-line 2kW converter. As we know this controller use current synthesizer to emulate off-time inductor current and so save one current sensor .What worries me is that the current synthesizer emulates the off time inductor current based on the input and output voltage and DC bias inductor value. So for case when the inductor swings significantly (for example from 100uH at full load to 400uH at no load) the current emulation error would be very high. In the other word, when we use the 400uH to calculate the RSYN then at full load when the real inductance is 100uH huge error in current emulation will be made which will affect current control. Can you please comment on this?
Thanks